You are here: Describing KAS Graphical User Interface > Windows and Panels Overview > Watch Window > Force a Variable

Force a Variable

At run-timeIn computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running, all variables in the table widget are animated 1 To better track variables and expressions of the PLC programs in test mode, the KAS IDE dynamically computes their value along with the execution and displays the result with real-time values.

You can double-click on the value of a variable (or press the ENTER key when it is selected) to open a pop-up window that allows you to:

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™